FB#.SELECT

Description

FB#.SELECT sets the feedback type manually (see FB#.IDENTIFIED ) or allows the drive to automatically identify the feedback type on power up.

Power Supply Notes:

If FB#.SELECT = -1, the power supply only turns on during the initialization phase. If the feedback type cannot be automatically detected, the power supply is turned off, and remains off until an AXIS#.CLRFAULTS is issued (which restarts the FB initialization), or FB#.SELECT is manually set to a specific feedback type.

When FB#.SELECT is manually set to a specific feedback type, the FB power supply remains on, unless a short is detected. This is useful for encoder types requiring calibration.

FB#.SELECT Input Values

Changing these input values manually sets the value of FB#.IDENTIFIED .


  • If the feedback setting fails, FB#.IDENTIFIED is automatically set to 0 (no feedback identified).
Type Description Notes
45 SFD3

Smart Feedback Device Gen 3

47 SFD-M SFD-M (Smart Feedback Device Gen M)

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000
Feature Change 02-06-03-000 Added SSI feedback type (36).
Feature Change 02-07-05-000 SFA-connected feedbacks (130, 131, 132, 133, 141) will also be auto-identified.
Feature Change 02-12-01-001 Added BiSS-B Digital types (35, 135).

General Information

Type

Read/Write

Units

N/A

Range

FB1 & FB2: -1, 1, 45, 46, 110, 111, 112, 120, 121, 130, 131, 132, 133, 134, 135, 136, 140, 141

FB3: -1, 1, 10, 11, 12, 13, 14, 20, 21, 30, 31, 32, 33, 34, 35, 36, 40, 41

FB4: 1, 11, 13, 14

FB5: -1, 1, 11, 13, 14, 31, 34, 35, 36

Default Value

FB1 & FB2: -1

FB3, FB4, & FB5: 1

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.SELECT

3500h

01h

Signed16

-

-

Read/Write

No

FB2.SELECT

3501h

01h

Signed16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30040

1

30040 (0x7558)

FB1.SELECT

Signed16

Read/Write

Yes

30041

1

30041 (0x7559)

FB2.SELECT

Signed16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.SELECT

30040

Signed16

Read/Write

-

FB2.SELECT

30041

Signed16

Read/Write

-